Post Go back to editing

ad8495在强电环境下的输入保护问题

你好

      我现在使用ad8495来检测K型热电偶的温度输出,K型热电偶放置在加热石墨炉中,加热石墨炉两端是大功率加热变压器的2个电极。K型热电偶在运行过程中,可能会因为一些原因在特定情况下接触到加热电极(不可避免),这就会导致加热变压器的输出副边的快速高压干扰电脉冲串通过热电偶泄漏到ad8495的输入端。出现这种情况时,ad8495就会被损坏,即使ad8495的2个输入都加入了RFI保护电路和二极管钳位电路,以及正负输入端的背靠背二极管保护电路。分析来看,加热变压器的输出副边虽然是4V,2000A的低压交流电,但其副边还是会有泄露的快速高压干扰电脉冲串,脉冲串的高压约为几百V,上升时间在几百ns级;二极管钳位电路所用的低泄露二极管如BAV199的反应时间都在微秒级别,起不到保护作用。

     目前我用ADG5412F放置在ad8495的2个正负输入前端,作为强电和esd干扰的防护措施,请问这种是否能保护ad8495不被击穿,或者adi官方有没有其他的这种在快速高压干扰电脉冲串环境下的保护电路?