Post Go back to editing

LTC2991的应用问题

如下三个问题需要答复:

1、采样电阻的选取标准问题(数据手册上对采用电阻选取的描述存在前后矛盾)

1.1文档建议按如下描述选取

1.2而后面给的典型应用没有按这个规则选(此处选的是0.01,而不是0.03)

疑问:采用电阻是按什么方法选取的??

2、电流的计算

如下图中 15.54mA/LSB 是怎么计算出来的,我计算的值是15.26mA/LSB=19.075/0.01*8

3、选用LTC2991采集电流(12V供电)的应用时,对分压电阻的选择,以及PCB layout有什么注意事项吗?就比如我选的采用电阻值很小0.002Ω。

Parents
  • 你好,

    关于你的问题解释如下:

    1. 如数据手册所述,0.03 ohm是该条件下最大采样电阻值,并不是强制要求。如果比较关心采样电阻上面的功耗问题,就会选择<0.03ohm的采样电阻,这个和计算规则不冲突。

    2. 我们计算并确认了一下,数据手册中给出的15.54mA/LSB是一个打印错误,感谢您指出这个问题,下一版数据手册会更新。

    3. 分压电阻的选择应该是在ADC输入范围内选择的尽可能大,但是如果对采样电阻的功耗比较敏感,可以适当减小采样电阻值,分辨率满足您的应用需求即可。输入共模电压也要在芯片VCC范围内,以免导致芯片内部ESD二极管导通影响芯片正常工作。还有一个就是像你看到的这个应用这样,使用分压电阻把V1 和V2引脚的输入采样电流降低,减少采样电流带来的误差。PCB layout你就参照数据手册11页的说明就可以。

    Best Regards,

    Jon

Reply
  • 你好,

    关于你的问题解释如下:

    1. 如数据手册所述,0.03 ohm是该条件下最大采样电阻值,并不是强制要求。如果比较关心采样电阻上面的功耗问题,就会选择<0.03ohm的采样电阻,这个和计算规则不冲突。

    2. 我们计算并确认了一下,数据手册中给出的15.54mA/LSB是一个打印错误,感谢您指出这个问题,下一版数据手册会更新。

    3. 分压电阻的选择应该是在ADC输入范围内选择的尽可能大,但是如果对采样电阻的功耗比较敏感,可以适当减小采样电阻值,分辨率满足您的应用需求即可。输入共模电压也要在芯片VCC范围内,以免导致芯片内部ESD二极管导通影响芯片正常工作。还有一个就是像你看到的这个应用这样,使用分压电阻把V1 和V2引脚的输入采样电流降低,减少采样电流带来的误差。PCB layout你就参照数据手册11页的说明就可以。

    Best Regards,

    Jon

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.