Post Go back to editing

HMC253AQS24ETR在使用中发现通道信号不稳定

1、最开始发现的时候是低温测试发现串读,拿出来完全恢复常温后,也表现串读,用烙铁重新焊接一下开关芯片后,常温不再复现,怀疑焊接不良,改好的两套再扔进低温箱里测试。

2、剩余9套和筛选是好的2套,照X光,焊接良好未有问题。现场重新焊接两个板子,还是串读,并且好的板子再次不好,也表现串读。同事反映低温再放进去的还是有串读的时候。所以焊接不良结论不对。

3、对比测试阻抗表现,焊掉接收端663,在TXN-P两端测试,好的板子,13.56MHz13.137MHz13.892MHz,分别为34+j1526+j941+j198个通道之间阻抗值相差不大;全串的板子分别为27-j1023-j1429-j10,全部呈容性;再找一个好的板子:31+j1419.8+j1958+j38,和第一个好的板子有一定差异;将全串的板子更换好板子的开关芯片,34+j3321+j1862+j33,再次表现感性,但是值和前两个板子还是有差异;

4、测试串读情况,2个好的板子,其中一个好使不串读,另一个串读,全串的板子更换好板的芯片后测试,2通道和3通道互串,5,6,7,8互串。

5、再找一个串一半的板子,再复测发现全都串,和之前表现不一样,更换第一批次天线板的ADI原厂提供的样品开关,不再串,再将问题开关换回来,还是串可复现。

6、之前筛选的好的板子,再测试两个,有不同程度的串读。

8、工作时测试TXN-P的电流,有串读的板子,串读通道放标签,91.8-87.8mA,不放标签时表现的都一致,76.5-72.5mA,;好板子不串读,放标签的通道电流和有串读的基本一致,不放标签的通道和有串读的板子表现也一致;通过计算假设按照峰值电流150mA,电压5V计算,功率值也不超过规格书的隔离度限值。在第一级开关前并联的270pF再增加一颗560pF电容,增大负载阻抗,降低电流,实测还是串读,此时的电流减小到了50mA左右;再并联一颗560pF,电流不再降低,因为电容值达到一定量级,不再有调谐作用;将叠层电感更换成绕线电感,感量不变,测试仍然串读。

 

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.