Post Go back to editing

小信号输入AD633时的问题

现在有一个幅值变化的正弦信号,范围在1mV-5V。在仿真软件中设置待测信号为40kHz,相位为0,幅值3mV,参考信号为40kHz,相位为0,幅值1V,如图所示,实现一个相敏检波。此时AD633芯片输出为5.14mV,此时每次减小1mV,芯片的输出也几乎不变。想询问一下这种情况是为什么,,输入信号的最低幅值是芯片手册中哪个参数体现的。使用AD835的话在1mV附近就能保持较大的输出变化,但其信号输入范围为1V,无法满足输入信号幅值为5V时的情况。

Thread Notes