Post Go back to editing

ADG1406BRUZ不同通道输出电压问题

我使用了ADG1406BRUZ,S1~S16输入的是不同的电压,有正电压,有负电压。

当我进行通道切换时,输出电压(D28 PIN)出现了附件波形变动,详细如下:

上一个通道的输入电压是+9V左右,切换到下一个通道的输入电压是-1.5V。

+9V到-1.5V变化之间有一个+9V->-15V的跳变。

备注:我的回路VDD=15V,VSS=-15V.EN是常态5V电压。

请问以上输出现象是ADG1406BRUZ芯片正常的输出特性吗?

Parents Reply Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.