Post Go back to editing

adn4605怎么测试连通没有?

我使用ADN4605,所有电源Vcc,DV,Vtti,Vtto都是3.3V,寄存器0x7D XPT Headroom和0xBB Tx Headroom置1 读取正确。将所有输出都连接到一个输入上(Input3),寄存器0x54连接状态读到是03,Tx输出状态都是使能:0xFF,RXEQIN均衡器:3db,其他未描述的都是默认值。用示波器测试输入Input3的P和N都是3.3v,输出也都是3.3v,将输入的P连接到板子的gnd上,输出依旧是高,除了总电源电流增加了100多mA没有其他啥变化。给输入加1KHZ信号,输出依然是高没有动静。。。输入输出端各自的上下拉电阻使能或禁止同样没有变化。 问: 1。想单纯测验证连接情况,我将输入拉到gnd或给信号是否可行?或者该怎么操作? 2。从总电源电流观测来看,用写寄存器让4605复位的方法,写一次电流不减小,写第二次后电流才减小,这是什么导致的?