Post Go back to editing

AD8106使用问题6

继续上一次追问 2.240V直流电压,经过10KΩ电阻分别连接在IN0~IN15,状态控制引脚为

(CE=0 UPDATE=1 CLK=1 D4=1 D3=0 D2=0 D1=0 D0=0 A2=0 A1=0 A0=0 CLK=0 delay_us(1)  UPDATE=0 CLK=1 RST=1 输入IN0对应输出OUT0,OUT0电压2.241V),

(CE=0 UPDATE=1 CLK=1  D4=1 D3=0 D2=0 D1=0 D0=1 A2=0 A1=0 A0=1 CLK=0 delay_us(1)  UPDATE=0 CLK=1 RST=1 输入IN1对应输出OUT1,OUT1电压2.241V),

(CE=0 UPDATE=1 CLK=1 D4=1 D3=0 D2=0 D1=1 D0=0 A2=0 A1=1 A0=0 CLK=0 delay_us(1)  UPDATE=0 CLK=1 RST=1 输入IN2对应输出OUT2,OUT2电压2.241V),

(CE=0 UPDATE=1 CLK=1 D4=1 D3=0 D2=0 D1=1 D0=1 A2=0 A1=1 A0=1 CLK=0 delay_us(1)  UPDATE=0  CLK=1 RST=1 输入IN3对应输出OUT3,OUT3电压2.241V),

(CE=0 UPDATE=1 CLK=1 D4=1 D3=1 D2=1 D1=1 D0=1 A2=1 A1=0 A0=0 CLK=0 delay_us(1)  UPDATE=0  CLK=1 RST=1 输入IN15对应输出OUT4,OUT4电压2.168V):

在这种控制状态下,测量IN0~IN14引脚量电压值为2.241V,但是IN15的引脚电压值为2.168V。总体感觉in15与in0-in14不同,这是什么原因?