型号AD8106,实际使用时遇到问题:
1、输入电压0V,IN0~IN14引脚量取电压值为0.001V,但是IN15的电压值为-0.156V,是什么原因?
2、输入电压2.240V,IN0~IN14引脚量取电压值为2.241V,但是IN15的电压值为2.168V,是什么原因?
型号AD8106,实际使用时遇到问题:
1、输入电压0V,IN0~IN14引脚量取电压值为0.001V,但是IN15的电压值为-0.156V,是什么原因?
2、输入电压2.240V,IN0~IN14引脚量取电压值为2.241V,但是IN15的电压值为2.168V,是什么原因?
我理解你的意思是说,输入信号的参考地接AD8106的地,输入2.240V信号给AD8106的IN0~IN15管脚,用万用表测量IN0~IN14管脚电压正确,IN15管脚不对,对吗?
这16个管脚没有区别的,输入阻抗为10Mohm,如果你的信号源是低阻抗输出,那么16个输入管脚应该是一样的信号。
尝试换一片AD8106试试?
我理解你的意思是说,输入信号的参考地接AD8106的地,输入2.240V信号给AD8106的IN0~IN15管脚,用万用表测量IN0~IN14管脚电压正确,IN15管脚不对,对吗?
这16个管脚没有区别的,输入阻抗为10Mohm,如果你的信号源是低阻抗输出,那么16个输入管脚应该是一样的信号。
尝试换一片AD8106试试?