Post Go back to editing

AD8362在输入两个载波时功率测不准的问题

    当在AD8362输入端输入一个纯载波(频率为2.001MHz,功率为10dBm;或者10dBm频率为2.0016MHz)时,此时根据对应电压关系显示功率是很准确的,都是10dBm。如果用一个合路器将两个10dBm频率为2.001MHz和2.0016MHz的信号同时加入时(频率间隔600Hz,已经考虑合路器对信号的衰减,合路器出来的两个信号都是10dBm),测出检波器的输出电压只增加了61mV,即对应功率显示变为了11.2dBm,实际应该为13dBm,用安捷伦的功率计或者其它仪器测得功率都是增加了3dBm, 当频率间隔相隔超过1kHz或更大时测得总功率可以达到12.3dBm。频率间隔小了就会出现总功率下降的问题。请问是怎么一回事呢,谢谢解答。

Parents Reply Children
No Data