Post Go back to editing

关于ADF4156不能锁定的问题

Thread Summary

用户在使用ADF4156搭建PLL电路时遇到VCO输出频率不变的问题,原因是VCO的输入控制电压为0V。最终答案建议检查锁相环芯片和VCO的供电电压,确保参考输入信号满足数据手册要求,并检查环路滤波器输出的压控电压。此外,建议检查寄存器写入顺序和配置值,使用ADIsimPLL软件生成的参数和评估板设计的硬件电路应无问题。用户还应尝试修改R分频器以改变鉴相频率,观察输出变化。
AI Generated Content

近期使用ADF4156做一款发射机,在搭建PLL电路时,将配置程序写入时,观察MUX管脚(设置N分频输出和R分频输出)都能观察到频率为鉴相频率的周期性脉冲信号,但是VCO的输出频率一直不变,经测试,原因是VCO的输入控制电压一直为0V。使用ADISIMPLL软件进行仿真搭建的三阶无源环路滤波器,为什么没有将电荷泵的信号积分为要控制VCO的电压(2V左右)?另外,配置完毕MUX管脚(设置N分频输出和R分频输出)波形正确是不是说明晶振和配置程序都没问题?还应该怎么调试?弄了好久,请各位大侠解决

附件1为ADISIMPLL仿真文件;

附件2为选择的VCO;

附件3为MUX管脚R分频输出;

附件4为MUX管脚N分频输出.

attachments.zip