Post Go back to editing

关于ADF4156不能锁定的问题

近期使用ADF4156做一款发射机,在搭建PLL电路时,将配置程序写入时,观察MUX管脚(设置N分频输出和R分频输出)都能观察到频率为鉴相频率的周期性脉冲信号,但是VCO的输出频率一直不变,经测试,原因是VCO的输入控制电压一直为0V。使用ADISIMPLL软件进行仿真搭建的三阶无源环路滤波器,为什么没有将电荷泵的信号积分为要控制VCO的电压(2V左右)?另外,配置完毕MUX管脚(设置N分频输出和R分频输出)波形正确是不是说明晶振和配置程序都没问题?还应该怎么调试?弄了好久,请各位大侠解决

附件1为ADISIMPLL仿真文件;

附件2为选择的VCO;

附件3为MUX管脚R分频输出;

附件4为MUX管脚N分频输出.

attachments.zip
Parents
  • 您好!

    看了您的N Counter Output的示波器的波形图。脉冲频率为2MHz,为鉴相频率,并且占空比非常小,是由于N分频数越大,占空比会越小。这些现象都是正常的。此时,VCO输出频率应为鉴相频率的N倍猜对。如果输出频率不对,并且怎么改N分频数都不正确。那么建议您此时修改R分频器,改变鉴相频率,如1MHz或500kHz。这样改变了环路特性,看输出是否有所变化。

Reply
  • 您好!

    看了您的N Counter Output的示波器的波形图。脉冲频率为2MHz,为鉴相频率,并且占空比非常小,是由于N分频数越大,占空比会越小。这些现象都是正常的。此时,VCO输出频率应为鉴相频率的N倍猜对。如果输出频率不对,并且怎么改N分频数都不正确。那么建议您此时修改R分频器,改变鉴相频率,如1MHz或500kHz。这样改变了环路特性,看输出是否有所变化。

Children
No Data