Post Go back to editing

关于ADF4156不能锁定的问题

近期使用ADF4156做一款发射机,在搭建PLL电路时,将配置程序写入时,观察MUX管脚(设置N分频输出和R分频输出)都能观察到频率为鉴相频率的周期性脉冲信号,但是VCO的输出频率一直不变,经测试,原因是VCO的输入控制电压一直为0V。使用ADISIMPLL软件进行仿真搭建的三阶无源环路滤波器,为什么没有将电荷泵的信号积分为要控制VCO的电压(2V左右)?另外,配置完毕MUX管脚(设置N分频输出和R分频输出)波形正确是不是说明晶振和配置程序都没问题?还应该怎么调试?弄了好久,请各位大侠解决

附件1为ADISIMPLL仿真文件;

附件2为选择的VCO;

附件3为MUX管脚R分频输出;

附件4为MUX管脚N分频输出.

attachments.zip
Parents
  • 请您参考一下我的附件2、3、4.R Counter Output和N Counter Output用示波器测量脉冲应该对着呢。硬件电路参考评估板设计的,也没问题,用示波器测量供电及晶振都对着。我想说明的是我选的VCO附件2,输入阻抗为50pF,使用ADIsimPLL仿真,选择ADF4156,选择单一输出频率,小数分频,输出频率2.2505GHz,鉴相频率2MHz,参考晶振20MHz,5V电荷泵供电,模数选200,选择二阶无源滤波器,VCO特性如下:使用2 point,V1:0.5V,对应频率2220.6MHz,V2:2.5V,对应频率2260.6MHz,VCO输入容抗50pF。环路带宽选10KHz~100KHz之间,相位45°~50°之间。用该配置仿真结果总是提示VCO input capacitance too large for this design。或者Lock Detect output did not pass 2.5V。    是我的VCO选的有问题吗,请参考附件2看看我的VCO是否能用?使用该硬件配置能否得到锁定的结果?请您使用上述配置的ADIsimPLL仿真试试,将结果发给我。另外,环路输出能否将电荷泵输出电流积分得到2V左右的Vtune控制VCO?寄存器配置应该正确的,上边附件有。

    调了几个月了都没结果,真的很无助。试了各种方法,还是不能锁定。ADI_YU久仰您的大名,在论坛经常能看到您的回复,请您一定给解解惑,不胜感激

Reply
  • 请您参考一下我的附件2、3、4.R Counter Output和N Counter Output用示波器测量脉冲应该对着呢。硬件电路参考评估板设计的,也没问题,用示波器测量供电及晶振都对着。我想说明的是我选的VCO附件2,输入阻抗为50pF,使用ADIsimPLL仿真,选择ADF4156,选择单一输出频率,小数分频,输出频率2.2505GHz,鉴相频率2MHz,参考晶振20MHz,5V电荷泵供电,模数选200,选择二阶无源滤波器,VCO特性如下:使用2 point,V1:0.5V,对应频率2220.6MHz,V2:2.5V,对应频率2260.6MHz,VCO输入容抗50pF。环路带宽选10KHz~100KHz之间,相位45°~50°之间。用该配置仿真结果总是提示VCO input capacitance too large for this design。或者Lock Detect output did not pass 2.5V。    是我的VCO选的有问题吗,请参考附件2看看我的VCO是否能用?使用该硬件配置能否得到锁定的结果?请您使用上述配置的ADIsimPLL仿真试试,将结果发给我。另外,环路输出能否将电荷泵输出电流积分得到2V左右的Vtune控制VCO?寄存器配置应该正确的,上边附件有。

    调了几个月了都没结果,真的很无助。试了各种方法,还是不能锁定。ADI_YU久仰您的大名,在论坛经常能看到您的回复,请您一定给解解惑,不胜感激

Children
No Data