Post Go back to editing

求助,关于AD8302输出值不准的问题

大家好,最近在用AD8302做幅值,相位测量电路。我按照数据手册上面的典型电路进行连接。如附图所示:  


C1=C4=C5=C6=102;R1=R2=68欧;C3=101;
C7=104;C2=C8=103;R4=68欧;两路输入信号时相位相差180度,幅值相同为1伏的正弦信号。但在输出端。幅值比=1.07V;相位比=0.4V;结果不正确。检查电路了都没有发现什么问题。请大家帮忙看一下,是哪的问题被我忽略掉了。比较急,谢谢大家了!