如何实现AD9958和AD8349的接口电路,试了好久没有实现SSB。

AD9958工作在FSK模式,已经实现。需要正交上变频到2.4g,LO使用ADF4360-1,采用的是成熟电路。AD9958和AD8349的接口电路,试了好久没有实现SSB。我采用的办法是,调节AD9958的上拉电阻,使两个通道每个输出为0.6VPP。然后电容隔离直流偏置,通过电阻分压生成0.4v直流偏置,不知道方案可行性如何。