Post Go back to editing

ADL5523的S参数仿真问题

向各位大师求解:

    ADL5523的S参数仿真问题。我现在用ADL5523的S参数文件进行ADS的仿真,S参数写的是三端口器件,1端口—RFIN,2端口—bias,

3端口—RFOUT。

   现在我仿真如图ADL5523仿真。数据图如图ADL5523数据图;

提问:

        (1)仿真时为什么测S(2,1)也有那么高的增益?(2端口不是偏压端口吗?)

         (2)我仿真时是不是要测S(3,1)的增益呢?(也就是说3端口就是RFOUT?)

          (3)如果2端口是bias端,那么如何连接呢?是不是按照ADL5523文档参考文档来连接电路?

attachments.zip
Parents
  • 您好!

    对于S参数及端口问题,产品线工程师答复如下,供您参考。

    I think the zip file is more accurate. The bias port also mean power supply pin of Vpos.

    The step size in the zip file is 100MHz. The data swept from 100MHz up to 4GHz.

    对于具体设计,建议您参考数据手册中TUNING THE ADL5523 FOR OPTIMAL NOISE FIGURE章节。ADL5523为低噪放产品,对于其使用,一般应用来说,优化噪声系数要重要与增益的调试。

Reply
  • 您好!

    对于S参数及端口问题,产品线工程师答复如下,供您参考。

    I think the zip file is more accurate. The bias port also mean power supply pin of Vpos.

    The step size in the zip file is 100MHz. The data swept from 100MHz up to 4GHz.

    对于具体设计,建议您参考数据手册中TUNING THE ADL5523 FOR OPTIMAL NOISE FIGURE章节。ADL5523为低噪放产品,对于其使用,一般应用来说,优化噪声系数要重要与增益的调试。

Children
No Data