Fref=10MHz
寄存器数据依次:
R7:7
R6:6
R6:800006
R5:5
R5:800005
R4:01800004
R3:3
R2:0F108002
R1:01890001
R0:3017C020
结果为:锁定,但是相位噪声很差,见附图。
保持其他不变,改R4:00000004,失锁;
另在R2=1F108002时均失锁。
保持其他不变,改R2:0F408002(R1、R0作相应改变),锁定,但相位噪声稍差,1k、10k不到90;之后更改R4为:00000004,失锁
保持其他不变,改R2:1F408002(R1、R0作相应改变),无论R4为00000004还是01800004,都是锁定,相位噪声同上,只不过10MHz谐波出现在±10MHz、±20MHz幅度不太一样。但是注意到R2 DB28 手册写道 It cannot be used if the phase detector polarity is set to negative.