Post Go back to editing

ADRF6655评估板问题

各位好!

我打算使用ADRF6655作为上变频混频器。ADRF6655的数据手册说,“The standard evaluation is configured for downconversion applications."那么,评估板可以用作上变频应用吗?我的射频频率设计为1700MHz,中频输入为200MHz.

谢谢!

  • 您好!

    如果您输出为1700MHz,那么ADRF6655不太适合您的应用。根据数据手册第11页图16,在upconversion模式下,输出频率到1610MHz时增益已经有了约3dB的衰减。建议您考虑使用ADL5801。

  • 您好!

    我查看了ADL5801的数据手册,

    第1:,这是ADL5801在900 MHz输出匹配下的上变频器模式,增益似乎也不好;

    ,这是在2.1 GHz输出匹配下的上变频器模式。请问“2.1 GHz输出匹配下的上变频器模式”和“900 MHz输出匹配下的上变频器模式”,是什么意思?

    第2:ADL5801是一个有源混频器,我还需要提供一个本振吗?请您给我推荐一款本振的芯片。我之所以想到ADRF6655,是因为它集成了PLL 和VCO,更方便一些。

    谢谢!

  • 您好!

    根据数据手册中,ADL5801上变频时可达到3GHz。具体描述请见下描述。

    For upconversion applications, the mixer load can be matched using off-chip matching components. Transmit operation up to 3 GHz is possible. See the Applications Information section for matching circuit details.

    如果您想选一款集成VCO的小数N分频锁相环产品,您可以考虑使用ADF4351。