AD8346使用疑问

1、调制器

1)AD8346是否可以用作UQPSK调制,如何实现UQPSK调制?是否可以通过改变基带信号的幅度来实现I、Q的幅度比?

2)是否可用作BPSK调制,即只使用I路或Q路,如果只使用一路时,另外一路输入该如何处理?

3)基带信号直流耦合还是交流耦合好?

4)调制基带信号频率为多少较好?基带调制信号直接是0频?还是低中频、高中频?

2、手册里讲:基带幅度为0.7V~1.7V,偏置电压为1.2V

1)请问是需要严格满足0.7V~1.7V,还是电平在此范围内即可?

2)偏置电压是否必须严格1.2V?大或小有什么影响?

3、本振

在设计中,本振由ADF4360产生,单端输出使用,经ETC1-1-13后,形成差分信号,但发现形成的I、Q两路本振信号输出幅度不一致,相差约2dB,经检查,原理图、PCB设计无误,IQ本振按照差分走线布线,可能的原因是什么?

烦请帮助解惑以上疑惑,谢谢!

Parents Reply Children
No Data