Post Go back to editing

AD9361接收调试

我现在调试AD9361的接收,遇到一些问题,想和大家讨论下,我的问题为:

(1)rx 通道本振的锁定测试手段(除0x247和配置0x035外的其他方法),比如是否可以测量接收本振的信号。

(2)rx有没有自测试模式。

(3)在调试接收时,我用chipescope采集数据,没有信号输入时(采集为噪声),分析采集到的数据时,发现里面有5m的信号,且数据被压            缩。data_clk为20MHz,FDD,DDR模式。