ADF4360-9无输出信号


我最近在调试ADF4360-9,参考信号100MHz,PFD=1MHz,想要输出75MHz信号,可是上电后没信号输出,加上FPGA控制后还是不变,另外Pin13脚电压只有0.5V左右(手册上说应该是0.6V左右),还有就是L1,L2外部电感本来我按公式计算的是振荡频率应该在76MHz左右,可是振荡出来的频率只有8MHz,我怀疑是不是电路没有振荡,所以输出信号才不正确,还有就是是L1,L2外部电感不是不是要用线绕电感才启振???求大神解答啊啊啊啊啊,急急急急急急。。。

Parents Reply Children
No Data