ADF4360-9无输出信号


我最近在调试ADF4360-9,参考信号100MHz,PFD=1MHz,想要输出75MHz信号,可是上电后没信号输出,加上FPGA控制后还是不变,另外Pin13脚电压只有0.5V左右(手册上说应该是0.6V左右),还有就是L1,L2外部电感本来我按公式计算的是振荡频率应该在76MHz左右,可是振荡出来的频率只有8MHz,我怀疑是不是电路没有振荡,所以输出信号才不正确,还有就是是L1,L2外部电感不是不是要用线绕电感才启振???求大神解答啊啊啊啊啊,急急急急急急。。。

Parents
  • 你好,我们现在需要采用ADF4360-9进行锁相环设计,我们参考了评估板给出的原理图,也就是ug-106的第9页和第十页,但有些地方没有看懂,首先是电源部分,原理图将USB正5V电压通过ADP3300-3产生VDD和VVCO电压,分别给DVDD、AVDD和VVCO供电,但很奇怪的是为何要使用那么多的0欧电阻,如R1,R13,R24,R2和R27。另外,UG-106中第三页给出的PCB貌似和实物图不同,其中没有R39和D5,难道是焊在背面?同时,在参考原理图和PCB中,三阶的环路滤波器部分的R10的位置应该如何选择,即放在背面什么位置,对环路滤波器有没有影响啊?谢谢

Reply
  • 你好,我们现在需要采用ADF4360-9进行锁相环设计,我们参考了评估板给出的原理图,也就是ug-106的第9页和第十页,但有些地方没有看懂,首先是电源部分,原理图将USB正5V电压通过ADP3300-3产生VDD和VVCO电压,分别给DVDD、AVDD和VVCO供电,但很奇怪的是为何要使用那么多的0欧电阻,如R1,R13,R24,R2和R27。另外,UG-106中第三页给出的PCB貌似和实物图不同,其中没有R39和D5,难道是焊在背面?同时,在参考原理图和PCB中,三阶的环路滤波器部分的R10的位置应该如何选择,即放在背面什么位置,对环路滤波器有没有影响啊?谢谢

Children
No Data