Post Go back to editing

ADF4360-9无输出信号

Thread Summary

用户在调试ADF4360-9时遇到75MHz信号无输出的问题,即使使用FPGA控制和线绕电感L1/L2后仍未解决。最终确认可能是VCO的谐振点不对,且L1/L2必须使用线绕电感。建议检查供电、电感值和环路滤波器参数,确保SPI写入正常、参考输入正确以及VCO正常工作。
AI Generated Content


我最近在调试ADF4360-9,参考信号100MHz,PFD=1MHz,想要输出75MHz信号,可是上电后没信号输出,加上FPGA控制后还是不变,另外Pin13脚电压只有0.5V左右(手册上说应该是0.6V左右),还有就是L1,L2外部电感本来我按公式计算的是振荡频率应该在76MHz左右,可是振荡出来的频率只有8MHz,我怀疑是不是电路没有振荡,所以输出信号才不正确,还有就是是L1,L2外部电感不是不是要用线绕电感才启振???求大神解答啊啊啊啊啊,急急急急急急。。。

Parents
  • ,L1/L2已经换成线绕电感,可是还是不行???发现线绕电感值和环路滤波器参数也有关系。那在软件控制方面有没有什么特别要求了,它的时序我都是按datasheet写的,可是还是没结果,哎,调了好长时间了???下面是我的FPGA时序。还请大神不吝赐教啊!!!

Reply
  • ,L1/L2已经换成线绕电感,可是还是不行???发现线绕电感值和环路滤波器参数也有关系。那在软件控制方面有没有什么特别要求了,它的时序我都是按datasheet写的,可是还是没结果,哎,调了好长时间了???下面是我的FPGA时序。还请大神不吝赐教啊!!!

Children
No Data