Post Go back to editing

关于HMC769的寄存器配置问题

Thread Summary

用户尝试使用HMC769芯片生成8.8GHz单频点信号,但配置寄存器后芯片无反应,输出8.01GHz未锁定信号。最终答案指出HMC769的VCO频率范围为9G到10G,无法输出8.8GHz,并建议使用有源环路滤波器。伴随答案提到,如果Vtune电压低于5V,可以使用无源环路滤波器,但在8.8GHz频点下Vtune电压可能过低,导致PLL无法锁定。
AI Generated Content

您好,我在使用HMC769 芯片产生一个8.8GHz单频点信号时,

1)参考源为100MHz晶振,Hcmos输出波形。

2)环路滤波器是无源结构(采用ADF4351的滤波器结构),带宽50kHz。

3)CEN端口使用一个100k的上拉电阻与3.3V电源相连接,SEN采用了一个100k的下拉电阻

        通过3.3V单片机将下列寄存器配置参数输入HMC769中,但是HMC769无任何反应,频谱中一直是一个8.01GHz的没有锁定信号,所以,请教一下:(1)我的寄存器配置是否有问题?(由于寄存器中有很多参数不是太明白有何作用,所以很多参数都是采用默认配置,)

                        (2)如果单纯的控制CEN端口为低电平,SDI、SCK、SEN都悬空,HMC769的RFout端口是不是没有任何信号输出?(我的电路板中有一个8.01GHz的信号输出)

期待各位专家的指导!!!!

Reg01h=0x02000006;
Reg02h=0x04000002;
Reg05h=0x0aca8642;
Reg06h=0x0c003a7e;
Reg07h=0x0e0090ca;
Reg08h=0x1006dffe;
Reg09h=0x120064c8;
Reg0Ah=0x14000000;
Reg0Bh=0x1602c0c2;
Reg0Ch=0x18000032;
Reg0Dh=0x1a000000;
Reg0Eh=0x1c000000;
Reg0Fh=0x1e000004;
Reg03h=0x06000058;
Reg04h=0x08000000;