Post Go back to editing

ADF4360-0无法配置,muxout一直为1.1v

目前我是用fpga编写spi接口去配置ADF4360-0,但一直无反应。我的参考时钟是16Mhz,我有量过ADF4360那端REFIN波形,其有一个直流1.5v左右的偏置,然后交流Vpp在0.6V左右。然后我有将muxout配置成DLD,Dvdd,量测到的波形都是1.1v。现在我不确定是REFIN输入时钟不对,还是spi并没有配置成功。如果没有参考时钟输入,ADF4360可以完成配置吗?如果能,将ADF4360的muxout模式配置成Dvdd模式,该pin会输出3.3V高电平吗?

attachments.zip
Parents Reply Children
No Data