Post Go back to editing

多片AD9361接收通道射频域相位同步问题

请教一下论坛里的诸位大牛;

     我需要用多片AD9361接收5.8GHz的射频信号,如何保证多片AD9361的相位同步?因为AD9361的external LO只能支持70MHz至4GHz,不能满足5.8GHz的要求;如果多片AD9361采用内部本振的话能否实现其射频域的同步?如果可以实现的话,需要什么条件,有没有什么特殊的要求?有没有相应的参考设计?

     非常感谢!

Parents Reply Children
No Data