Post Go back to editing

AD9371的片间射频同步问题,希望得到解答。谢谢!

AD9361的user manual(UG570)文件的第87页有一段话:“IF the MCS RF Enable bit is set then the RF LO dividers will remain enable  in the alert state.this will allow for the RF phase relationship between multiple devices to remain constant thoughout operation.” 

从文意可知:虽然多片间做不到射频LO的相位相同,但是每次上电后,可以通过寄存器设置,保证片间的相位关系在工作过程中恒定。这样我们就有可能通过自检与校正将此固定的相位差在基带的处理软件中减掉。

我想问的是:AD9371的User manual(UG992)中并没对此有明确说明,但是是否也有类似的寄存器设置机制让片间的射频相位关系在工作中保持恒定?

这样就可以上电工作后校正一次就可以了,而不需要不停的校正。我认为这个特性对于应用非常重要,AD9361拥有的很有用的机制,在AD9371不应该没有了吧?这个问题对我很重要,也很迫切,希望能得到明确的解答。谢谢!