Post Go back to editing

RF Output Power with a wide band signal

Category: Datasheet/Specs
Product Number: AD9361

Question 1:

The maximum output power of the AD9361 for a single tone is 7dBm.

What would its output power be when transmitting a signal with a 10MHz bandwidth? How to calculate the theory power?

I did the following test:

Keeping the AD9361 configuration the same as for single-tone with a output power about 7dBm, I generated a 10MHz bandwidth signal and observed the marker power of approximately -27dBm on the spectrum analyzer. Is this reasonable?

I noticed that the power marked by the spectrum analyzer represents the total power for the RBW. Therefore, to calculate the total power of the 10MHz bandwidth signal, integration should be used. For example, if the RBW is 3kHz, then the total power is:

-27dBm + 10log10(10MHz / 3kHz) = 8dBm

This seems to correspond to the maximum output power of the AD9361 for a single tone.

Question 2:

Is the output power specified in the AD9361 manual the maximum integrated power across the channel?

  • The maximum power on the datasheet is for the CW signal, and the output power of the wideband signal is less than 7dBm, an external amplifier or gain block is often required to further amplify to the required power. -27dBm seems to be a little smaller, whether the output is connected to a balun or other circuit. The maximum output power corresponds to each individual channel and is obtained at 0dB attenuation.