Post Go back to editing

ADF4158/ADF4159/ADF4169底噪抖动及小杂散扫动问题

Category: Hardware
Product Number: ADF4158/ADF4159/ADF4169

各位工程师您好,最近项目上使用ADF4159+HMC510,出8.5GHz信号的时候,发现信号锁定后,频谱仪扫宽打2MHz时,底噪一高一低的抖动(疑似呼吸噪声),并且伴有小杂散来回扫动。在官网上查了一下,七八年前有其他工程师反馈过这个类似的问题。后来将ADF4159替换成ADF4169,问题未得到解决(后经反复实验寄存器参数,可以解决呼吸噪声的问题,但是来回扫动的小杂散还是存在,而且必须将电荷泵电流设置在1.25mA以下以及constant Neg Bleed设置为使能状态。只能说改善了,但是问题并没有正真的解决)。再将ADF4159替换成ADF4158,问题依然没有得到解决,请问大家有遇到过此类问题吗?有解决方法吗?望遇到过同样问题的同行告知解决办法,万分感谢

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.