ADI年度贺岁片——使用AD9851和ADL5350做射频电路的时候的问题

ADI年度贺岁片——使用AD9851和ADL5350做射频电路的时候的问题 by stevenC

        我做过的一个项目中需要用到一些射频器件,其中我使用到的有DDS:AD9851芯片;混频器:ADL5350;RF增益器件:AD8354;自动增益器件:AD8367。大概思路和射频收发器差不错,由DDS产生一个小步进的频率可调的高频信号,用混频器和PLL产生的高频信号混频、滤波后经过放大,驱动功放,在用一个功放期间放大功率后由双工器发送。接收的时候使用到了两次自动增益,然后送入DAC变成数字信号。

        思路看上去没什么问题,可是我只做到了混频这一步就做不下去了,因为混频之后产生了很多谐波和交调,需要的是433MHz左右的信号。滤波器使用的是ADS2011设计的LC滤波器,其实频率也不是特别高,我想应该用不着设计微带线的。可就是一直滤波失败啊。希望ADI的混频器datasheet也能够添加一些关于滤波的设计参考吧,呵呵

        使用AD9851的目的是产生中心频率为45MHz的高频信号,我手上有几块淘宝上买的评估版,测试了之后感觉9851做频率源真是太好了,要多少频率就做多少频率,可是问题又来了,理论上9851能够产生高达60MHz的信号,可是实际上我让它输出45MHz的时候波形就特别难看,而且用示波器测试出来的频率和我给的控制字计算出的理论频率相差太多了(其实也不多,但是在我的设计中频率是关键参数),给我的应用造成了一些麻烦。

        以上两个图是我用示波器观察到的波形,给的控制字是0X40022F3D,计算出来应该是45.006MHz,实际上测出来该时刻的瞬时频率是44.72MHz,相差了0.286MHz,当然示波器存在测量误差肯定是难免的,频率一直在45MHz左右变动。

        现在在写论文,正好写到这一部分了,顺便也研究了一下ADI的Analog Dialogue 第46卷第1期中Brendan Cronin写的关于DDS的文章,觉得很有学习价值。谢谢ADI。

  • Created
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.