English
EngineerZone
RF
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
RF
Cancel
RF
问答
讨论
文档
成员
标签
Cancel
Browse Our FAQs
Need Help? Ask a Question
Open Questions. Can you
help
?
AD9361调制问题
Not Answered
2 months ago
利用AD936X配置软件生成的脚本,AD9361 TX输出信号的频率和设置的频率不一样
Not Answered
6 months ago
This group hosts discussions and FAQs regarding RF. Please read the Analog Devices EngineerZone
Code of Conduct
before posting.
All Threads
by
AntaurZhang
RF
Latest
2 months ago
by
Echen5
351
1
0
Answered
AD9361中RFPLL时钟设置
0
Answered
在noOS例程中,设定RFPLL时钟频率时,调用函数 int32_t ad9361_rfpll_int_set_rate(struct refclk_scale *clk_priv, uint32_t rate,uint32_t parent_rate) 在这个函数中,计算分频系数前,调用了一个函数ad9361_from_clk() 这个函数是把频率扩大成2倍,这是个什么原因啊?
351
1
0
by
TerryChen
RF
Latest
2 months ago
by
Echen5
494
1
0
Not Answered
AD9361调制问题
0
Not Answered
基于pluto的AD9361的开发板,使用ZYNQ 7020处理器,发现调制的时候出现以下问题: 1. 设置LO为 1500MHz,工作在2T2R模式下; 2. IQ数据为:I为 1MHz 的cos,Q为 1MHz的sin; 2. 调制出来的结果是:1499MHz,而不是预期的 1501Mhz。 请教,问题出在哪里?
494
1
0
by
arosy
RF
Latest
2 months ago
by
Echen5
311
1
0
Answered
RF放大器 HMC1099
0
Answered
请教ADI的专家,HMC1099这颗芯片,采用28V供电,这颗芯片有 >10W@50Ω 的输出能力,换算后电压摆幅是否能达到约 63Vpp 输出RF信号,还是说只能输出不超过28Vpp的RF信号
311
1
0
by
cb1274
RF
Latest
5 months ago
by
Echen5
310
1
0
Answered
ADL5961的S2P文件
0
Answered
目前使用ADL5961芯片装贴后端口驻波较差,能否提供ADL5961的S2P文件,做信号完整性仿真,在官网上找不到; 或者有无其他类似的资料能够做 ADL5961的 信号完整性仿真。
RF Power Detectors
Wideband Transceiver IC
RF Integrated Transceivers
310
1
0
by
weaponddr
RF
Started
6 months ago
233
0
0
Not Answered
利用AD936X配置软件生成的脚本,AD9361 TX输出信号的频率和设置的频率不一样
0
Not Answered
你好,我在使用zedboard+FMCOMMS3-EBZ的开发板进行测试时出现了TX输出频率与设置频率不一样的情况,设置的频率为800MHz,输出的频率则为798.2MHz,频谱结果如下图所示。 在使用matlab支持的FMCOMMS3的硬件包的时候输出的频率是正常的,如下图所示。并因此排除是由于参考时钟导致的误差。 我想问下是我利用软件生成的脚本哪里出了问题吗?附上我生成的脚本文件。谢谢! //************************************************...
Wideband Transceiver IC
RF Integrated Transceivers
233
0
0
by
qsj
RF
Latest
8 months ago
by
刘国龙
967
2
0
Not Answered
ADF4158/ADF4159/ADF4169底噪抖动及小杂散扫动问题
0
Not Answered
各位工程师您好,最近项目上使用ADF4159+HMC510,出8.5GHz信号的时候,发现信号锁定后,频谱仪扫宽打2MHz时,底噪一高一低的抖动(疑似呼吸噪声),并且伴有小杂散来回扫动。在官网上查了一下,七八年前有其他工程师反馈过这个类似的问题。后来将ADF4159替换成ADF4169,问题未得到解决(后经反复实验寄存器参数,可以解决呼吸噪声的问题,但是来回扫动的小杂散还是存在,而且必须将电荷泵电流设置在1.25mA以下以及constant Neg Bleed设置为使能状态。只能说改善了,但是问题并没有正真的解决...
hardware
ADF4158/ADF4159/ADF4169
967
2
0
by
BayMax0916
RF
Latest
10 months ago
by
Echen5
494
1
0
Answered
ADF4159 AUX
0
Answered
If I intend to design an FMCW radar using ADF5901 and ADF4159, and I only want to use the AUX and RFINA in single-ended mode for connection, is this feasible? In this case, should the corresponding complementary AUX be left floating, and RFINB be grounded...
Microwave and mmWave Transmitters
RF Integrated Transmitters
rf & microwave
Fractional-N PLL
adf4159
adf5901
Phase Locked Loop (PLL) Synthesizer & Translation Loop
Show More
494
1
0
by
xiaoyide
RF
Latest
11 months ago
by
AntaurZhang
2530
4
0
Answered
请问AD9361的DATA_CLK和ADC COLCK RATE的关系
0
Answered
@@最近在调试AD9361的BBPLL,目前BB PLL 已经锁定。但不知道DATA_CLK这个时钟怎么配置?和ADC 的采样率有什么关系? 参考时钟为40MHz,配置的ADC CLK=30.72MHz,检查到 0x05E[7]==1,BBPLL锁定 。使用CLKOUT引脚输出ADC_CLK/2,用示波器在CLKOUT引脚可以测到15.36MHz的时钟。但是DATA_CLK引脚测得的时钟为1.92MHz,现在不知道DATA_CLK的时钟对不对,该怎么配置? 我想请问一下DATA_CLK和ADC...
ad9361
sdr
Wideband Transceiver IC
RF Integrated Transceivers
2530
4
0
by
jiachen
RF
Latest
over 1 year ago
by
Echen5
537
1
0
Not Answered
AD9361 的LO频率偏移
0
Not Answered
我最近在做卫星接收机 我在测试1561.098MHz的频点的时候,发现频偏,使用了官方的No os和官方的SPI寄存器纯PL端配置 都有频偏,频偏大小在不同使用AD9361的设备上 同一个配置文件 还不一样 使用fmccoms3+zedboard 偏移大于1e5Hz,使用别的设备同一个配置文件 偏移也有21000Hz,我想知道是什么导致了如此大的偏移 (使用DCXO还是external clock 40MHz)都是如此
ad9361
Wideband Transceiver IC
RF Integrated Transceivers
537
1
0
by
gchen
RF
Latest
over 1 year ago
by
zuohufa
899
2
0
Not Answered
AD9361接收时延不稳定,如何让接收时延固定?
+2
Not Answered
我用 ZYNQ+AD9361 的架构进行直扩信号自收发(外部将 AD9361 发射的信号环回至接收端), AD9361 的配置在 PS 侧,参考时钟为 40MHz ,采样率为 20MHz 。在外部条件不变的情况下, PS 侧重新启动应用程序(配置 AD9361 ),会导致测距值发生跳变,跳变值为 data_clk 周期的整数倍,且不固定;将 AD9361 的接收频点或发射频点中的任一值改变,让信号失锁,再将接收频点或发射频点改为原来的值,重新锁定后,也会导致测距值发生跳变,跳变值为 data_clk...
899
2
0
View All Threads
by
arosy
RF
Latest
2 months ago
by
Echen5
311
1
0
Answered
RF放大器 HMC1099
0
Answered
请教ADI的专家,HMC1099这颗芯片,采用28V供电,这颗芯片有 >10W@50Ω 的输出能力,换算后电压摆幅是否能达到约 63Vpp 输出RF信号,还是说只能输出不超过28Vpp的RF信号
311
1
0
by
cb1274
RF
Latest
5 months ago
by
Echen5
310
1
0
Answered
ADL5961的S2P文件
0
Answered
目前使用ADL5961芯片装贴后端口驻波较差,能否提供ADL5961的S2P文件,做信号完整性仿真,在官网上找不到; 或者有无其他类似的资料能够做 ADL5961的 信号完整性仿真。
RF Power Detectors
Wideband Transceiver IC
RF Integrated Transceivers
310
1
0
by
BayMax0916
RF
Latest
10 months ago
by
Echen5
494
1
0
Answered
ADF4159 AUX
0
Answered
If I intend to design an FMCW radar using ADF5901 and ADF4159, and I only want to use the AUX and RFINA in single-ended mode for connection, is this feasible? In this case, should the corresponding complementary AUX be left floating, and RFINB be grounded...
Microwave and mmWave Transmitters
RF Integrated Transmitters
rf & microwave
Fractional-N PLL
adf4159
adf5901
Phase Locked Loop (PLL) Synthesizer & Translation Loop
Show More
494
1
0
by
AntaurZhang
RF
Latest
2 months ago
by
Echen5
351
1
0
Answered
AD9361中RFPLL时钟设置
0
Answered
在noOS例程中,设定RFPLL时钟频率时,调用函数 int32_t ad9361_rfpll_int_set_rate(struct refclk_scale *clk_priv, uint32_t rate,uint32_t parent_rate) 在这个函数中,计算分频系数前,调用了一个函数ad9361_from_clk() 这个函数是把频率扩大成2倍,这是个什么原因啊?
351
1
0
by
LiangYingsheng
RF
Latest
over 2 years ago
by
zwang
647
2
1
Answered
DC Blocking capacitors
0
Answered
HMC252A带宽支持直流信号,为什么数据手册上说输入输出端要加隔直电容?
SP8T
spdt
hardware
spst
hmc252a
SP6T
SP5T
sp4t
RF Switches
SP3T
Show More
647
2
1
by
wanghahaha
RF
Latest
over 2 years ago
by
Jackie Wang
903
1
0
Answered
AD9361的data_clk与参考时钟相位不锁定
0
Answered
我使用的参考时钟为40MHz,且同一个时钟晶振产生pps信号,我的目标是40.92MHz采样率下让data_clk与该pps信号有对齐的相位(固定的相位差); 我发现配置采样率为40.92MHz的时候通过示波器观测到的data_clk与pps信号相位不固定,data_clk约为163.6MHz(可能示波器有误差),将data_clk通过4分频后可以得到我想要的40.92MHz时钟(示波器频率准确),这个时钟信号同样不能与外部pps信号同步; 如果我配置采样率为40MHz,则上述 data_clk为160MHz...
903
1
0
by
xianbinrao
RF
Latest
over 9 years ago
by
孙治国
2088
1
0
Answered
AD9371几点疑问
0
Answered
如图,想咨询AD9371几个问题,AD9371感觉对用户开放的资源太有限了,目前存在几点疑问 1,当前我用的是125M的参考时钟,但是上电初始化的bin文件无法校验过去,但是如果在配置参数设置采样率为官方的122.88是可以正常校验的,只是会出现通过内部切换频率不准的情况(因为我的参考时钟是125mHZ),但是我看手册上的那个9528也是可以配置125MHZ,我的疑问是那个BIN文件和采样率有关联的嘛?如果有关联应该如何修改呢,因为用户手册上对BIN文件没有相关的说明。 2,ad9371的频率切换时间和AD9361相差太大...
ad9371
Wideband Transceiver IC
RF Integrated Transceivers
2088
1
0
by
Zhiwei
RF
Latest
over 9 years ago
by
ADIApproved
5396
1
0
Answered
AD9371的AD与DA采样率
0
Answered
想问一下AD9371的AD与DA采样率各是多少?有没有相关的用户手册?
ad9371
Wideband Transceiver IC
RF Integrated Transceivers
5396
1
0
by
johnny.chen
RF
Latest
over 2 years ago
by
caicai
4390
3
0
Answered
经过AD9361之后的波形失真问题
0
Answered
原始波形,两路一样,只是有相位差 经过AD9361之后的波形 求大神分析下有可能是什么原因造成的,增益?滤波器? 不甚感激
4390
3
0
by
menghao
RF
Latest
over 9 years ago
by
ADIApproved
1807
2
0
Answered
AD9361 tx secondary filter resistor and capacitor
0
Answered
请问AD9361 tx secondary filter resistor and capacitor寄存器(0x0D1和0x0D2)该怎么配置呢,没有从手册中找到具体的配置方法。 谢谢!
ad9361 寄存器*
ad9361
Wideband Transceiver IC
RF Integrated Transceivers
1807
2
0
View All Threads
更多内容
Post
Go back to editing
Filter
Show More
Before You Switch
Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.