客户使用情况:目前在使用贵司的ADF4351产品,但是在归一化1/f噪声这个参数测试时,测试的指标只有-112DBC/HZ,比贵司的DATASHEET指标低6DB,我使用的条件是:1、自己绘制的PCB板,RO4003板材;2、采用贵司LDO,HMC1060供电,使用的参考100MHZ,相位噪声-145DBC/HZ @1KHZ;3、ABP = 3 ns,PFD:50mhz ,RF:4004MHz;4、测试RF相噪 -100DBC/HZ@10KHZ;5、通过贵司提供公式:PN = PN1_f + 10 log(10 kHz/f) + 20 log(fRF/1 GHz),计算得到归一化1/f噪声:-112DBC/HZ,测试出的值与DATASHEET有一定差距。
我想知道贵司在ADF4351这款产品,在归一化1/f噪声这个参数测试时,使用的测试条件是什么,劳烦说明具体一点,谢谢!RF和Microwave (HMC系列产品问题存档)analogchina-adminADIemployeeanalogchina-admin