关于比较器HMC674的工作方式问题

     您好,想请教ADI大神一个问题,最近在找一款比较器,输入有效信号幅度为2mv~2V,可设定,脉冲宽度200~300ps,上升/下降沿70ps的脉冲信号;现需要转化成脉冲宽度不大于5ns,上升/下降沿不高于100ps的TTL或者CMOS信号,可供后端处理;

     现在找到比较器HMC674基本满足要求,但是看了下资料没有太明白其工作方式,按照我对比较器的理解,应有一个参考电压供比较参考,然后可以对应输出高低电平(运放搭建的比较器电路);但是此款芯片没有看懂具体是怎么工作的?难道是直接对输入脉冲信号进行对应输出吗?但是也应该有个参考电压值吧,比如何时跳变电平状态?难道是有边沿就可以吗?另外其LE锁存端怎么用?引脚VTP、VTN怎么用?本人能力有限,还望ADI专家指点一下,不胜感激!