how to calculate the Active loop filter parameter when I use HMC702 and HMC733 with HMC492 to generate a signal of 16GHz? In my design,the PFD is 60MHz with the reference frequency 120MHz.Must I change the Kv of the VCO when I use the Hittite PLL  eva

使用HMC733和HMC702和分频器HMC492产生16GHz的信号,参考频率 120MHz,鉴相频率60MHz。我计算环路参数的时候需要将Kv除以2吗?因为VCO输出的频率经过功分和分频之后返回到HMC702的VCOIN端。