Post Go back to editing

HMC952A的供电电压

Thread Summary

The user inquires about the HMC952A's 4 gate voltages and 3 drain voltages, and how to power them. The final answer specifies that VDD can be 5V or 6V, and the gate voltage range is -3V to 0V. Accompanying answers seek clarification on whether VDD1 to VDD4 and Vgg1 to Vgg3 can be connected together and the power-up sequence, as well as the use of external op-amps on pin 12 and 13.
AI Generated Content

请问HMC952A怎么有4个栅压,3个漏压啊,应该如何供电啊。求指导?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.