Post Go back to editing

HMC412B调制微波脉冲损耗问题。

HMC412B调制微波脉冲损耗问题。

您好,我使用该混频器作为微波脉冲调制器,在LO给10GHz,10dBm的本振信号,在IF给20ns宽度200us周期250mV脉冲,在RF口测得的脉冲功率只有-5dBm(频谱仪zerospan同步触发)。为何转换损耗如此之大?有没有办法做小?另外手册说IF电流最大+-6mA,我已经给到5mA了,但是我作为脉冲调制应用是不是可以更大一点呢?比如20mA。有篇文章这么说的,如下,链接为http://www.emhiser.com/images/content/121/ETTI-_Mixer_Application_Guide.pdf

求高手解答。谢谢!

Parents Reply Children
No Data