Post Go back to editing

关于参考电路CN0174

Dear:

   最近看到参考电路CN0174《使用有源环路滤波器和RF预分频器的低噪声12 GHz微波小数N分频锁相环》,看到其12 GHz PLL 的测量性能与仿真相位噪声性能对比图。我不知道,在设定的参数下,是如何仿真得到在12GHz输出时相位噪声达到-130dBc/Hz@1kHz。如果相噪按6dB倍频恶化,从100MHz参考输入,鉴相频率25MHz,算上ADF5001的预分频系数,12GHz频率分频到鉴相频率,共有480次分频。这种情况下,相位噪声是如何实现或如何计算仿真到图示中的性能的??文中ADIsimPLL仿真设计文件链接已失效,求解仿真及实现过程。求指教。

CN0174.pdf