ADRF6602无法控制

       你好,我现在调试芯片ADRF6602,5V供电,上电后电流大概0.27A。

问题1 是上电在端口LON,LOP测试初始振荡频率大概是在2.2G左右,当写入控制字后,振荡频率变为3.4G左右,电流变为0.16A,根据内部LO的频段1550-2150MHz(这个频点是经过VCO  2  分频的吗?),当我重新断电后,上电频率也是2.2G左右,但是写入控制字后就没有振荡频率了,电流也变为了0.05A,经测试,2脚电压为0,(前后两次写入的程序相同),上诉两种情况都会出现,我曾将MOUXOUT引出参考信号,但是没有实现。

       问题2 是ADRF6602的环路是通过一个电源的bypass电容接地的,这和我们普通的环路直接到地有什么优势吗?程序逻辑时序如附图。望解答,谢谢。

attachments.zip