HMC830调试问题

1.咨询HMC830评估板是否设置了滤波器限定了频率输出,我们设计希望测试900M-1.2GHz输出,但是测试评估板却发现只能输出3GHz信号?设置了分频器,但是不影响输出,请帮助确认?

2. ADI和Hittite官网可以下载HMC830EVB原理图,是否可以申请PCB版图文件辅助设计?

3. 设计跳频输出,间隔1MHz,是否要用到VCO Auto-Calibration (AutoCal)功能,是否需要先设置Reg 05h: for AutoCal transfers switch control data to the VCO subsystem via Reg 05h. 该功能是否参考pll_operating_guide_rf_vcos文档4.2  VCO Calibration?

谢谢!

1. 没有滤波器,可以全频率范围输出,确认你的寄存器配置是否正确;

2. 不提供版图;

3. 需要auto Cal功能打开

前辈  您好  请问”频点输出只能3G”的问题解决了吗  如何解决的  我现在也这个问题

This document was generated from the following discussion: HMC830调试问题

  • Created
  • Updated
Was this helpful?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.