Post Go back to editing

MAX22513- VIL、VIH

Thread Summary

The user inquired about potential errors in the Vrstil and Vrstih values in the MAX22513 product documentation. The final answer suggests that the input voltage below 0.8V is recognized as low (L), and above 3.05V as high (H), and the support engineer will confirm this further.
AI Generated Content

 在MAX22513产品说明文档中Vrstil、Vrstih这两个数值是不是出现了错误?