Post Go back to editing

看手册AD9959是否在任何频率输出时相位均有0.022度的控制分辨率?

        按照手册Φ=(POW/16384)*360公式计算,AD9959两通道正弦波之间相位差最小可以有0.02197度的精度,但我实际使用时幅度、频率均可实现手册分辨精度,但相位实现精度却与手册相差较大:如AD9959输出1MHz时怎么调节相位偏置字都远达不到0.022度的手册精度,只有频率降至100Hz时才能实现较明显的两通道间相位差分辨率。

        难道我理解AD9959在0.001Hz-200MHz任何频率输出时,两通道正弦波相位差可从0.022-360度任意调整有误?是不是AD9959输出频率越高,通道正弦波相位实现精度就越低?举例说明:100Hz时两通道正弦波之间可以实现最小相位差0.022度,但随着输出频率的增高,如1MHz时两通道正弦波之间可以实现最小相位差就是几度甚至几十度?本人仔细想想AD9959片内余弦角度对应幅度数据表应该有16384的分辨率,当时钟频率一定时,输出频率越高对应数据表抽出的是否就越少,相位分辨率就会相应越低,我推测的是否正确?