给芯片上电后,各电源引脚电压正常,用示波器看不到晶振引脚的波形。晶振两个引脚都是大约0.8V电压,SYNC_CLK也看不到波形。晶振用的是25M无源晶振并两个39pF电容。请教各位这是什么原因呢?不胜感激。
给芯片上电后,各电源引脚电压正常,用示波器看不到晶振引脚的波形。晶振两个引脚都是大约0.8V电压,SYNC_CLK也看不到波形。晶振用的是25M无源晶振并两个39pF电容。请教各位这是什么原因呢?不胜感激。
将芯片reset,并通过寄存器设置PLL的相关参数,如分频比,CP电流,VCO范围等,对应的硬件焊接PLL的环路滤波器电阻电容。
请问PLL环路滤波器怎样配置?晶振25M,倍频20,非常感谢!
请您核对一下CLK_MODE_SEL引脚的电平。关于环路滤波器,请这样连接引脚27:
Connects to the external zero compensation network of the PLL loop filter.
Typically, the network consists of a 0 Ω resistor in series with a 680 pF capacitor
tied to AVDD.
我的情况和楼主的相似;给芯片上电后,各电源引脚电压正常,用示波器看不到晶振引脚的波形。SYNC_CLK也看不到波形。晶振用的是25M无源晶振并两个39pF电容。不同的是晶振两个引脚都没有电压。请问是什么原因?多谢!