Post Go back to editing

ADN2915 recover clock full rate output can reach 10GHz?

My data rate is 10Gbps,and I want to output recover clock which is 10GHz(SDR) ,meanwhile I don't want the output data,I only need the  recover clock.

Can I use the register OUTPUTA.D2=1 (DDR clock disabled) ?

From Figure 1  : BLOCK DIAGRAM ,if close the DDR function ,I would  achieve goal. 

Thanks!