Post Go back to editing

使用AD9910内部的PLL发现有串扰信号

我用AD9910做了块板子,使用AD9910内部的PLL,参考时钟为10MHz,64倍频,输出80MHz,发现在70MHz和90MHz处有串扰信号,幅值与80MHz差65dB。怀疑是AD9910的PLL引起的。后来借来一块AD9912的评估板,发现同样问题。请问有办法消除这种串扰吗?谢谢!

Parents Reply Children
No Data