Post Go back to editing

关于信号上升时间的延迟

您好:

我使用STM32的GPIO产生一个阶跃信号,信号的上升时间在直接测试GPIO时为5ns左右,我后面接了一个TI的CD74HC4053芯片进行通道选择,当GPIO为高时,输出3.3V电压,当GPIO为低时,输出0V电压。控制信号使用GPIO产生的阶跃信号。然而,在接上后续IC后,上升时间会变长。请问ADI有没有这种高速的通道选择器件,要求在50ns以内。

谢谢

Parents Reply Children
No Data