Post Go back to editing

请教:AD9957 芯片同步问题?着急啊!求回复!谢谢!

1. 在使用过程中,发现AD9957同步输出信号 SYNC_OUT的频率比数据页上的公式计算值大一倍,比如差值系数R=10,sysclk=1GHz,在QDUC模式下,按公式应该为1000/32*R=3.125MHz,可实际输出为6.25MHz,改变差值系数R,输出也跟着改变,但输出始终大一倍。在该模式下,PDCLK的输出跟公式一致,所以我觉得R寄存器的值写入应该是正确,不知是何原因?

2.SYNC_SMP_ERR同步采样错误指示引脚,在同步验证模块复位状态下为0,在使能状态下,在同步信号SYNC_IN引脚无输入时,该引脚为0,有输入时为1,可看数据页上是该引脚为1表示同步错误,所以想确认下,这种想象是否正常?

谢谢!

消息编辑者为:xiaobing

Parents Reply Children
No Data