Post Go back to editing

求教AD9910和AD9956的REFCLK输入功率要求

Thread Summary

The user inquired about the minimum REFCLK power requirement for AD9910 and AD9956 in dBm and the corresponding peak-to-peak voltage. The final answer stated that the thread was closed and assumed answered. An accompanying answer clarified that the REFCLK input impedance is not 50 ohms, making power representation unclear, and recommended checking the chip manual for voltage peak-to-peak requirements.
AI Generated Content

请问AD9910和AD9956的REFCLK 单端 输入时最低功率要求多少dBm,用峰峰值电压表示分别是多少。因为我看9956的数据手册给出了两种表示方法,但最低功率和最低峰峰值电平之间按公式转换两者不相等,最大功率和最大峰峰值电平之间按公式转换是相等的。9910只给出的是峰峰值电平要求,最低峰峰值电平按公式转成功率是-22dBm,是不是太低了。盼回复!!

另:为什么REF的要求一般以峰峰值电平表示,我看锁相环的也是这样,为什么不直接以功率表示不是更直观吗?

attachments.zip