English
EngineerZone
时钟和DDS
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
时钟和DDS
Cancel
时钟和DDS
问答
AD9910出现二次谐波原因?
问答
讨论
文档
成员
标签
Cancel
Thread Details
State
Verified Answer
Replies
12 replies
Subscribers
35 subscribers
Views
2773 views
Users
0 members are here
Options
Share
More
Cancel
Related
Post
Go back to editing
AD9910出现二次谐波原因?
111111
on Sep 5, 2013
Thread Summary
用户询问关于AD9910在输出10MHz信号时出现20MHz谐波的问题。最终答案建议用户参考AD9910评估板的原理图和滤波器设计,以解决谐波过高的问题。用户反馈在低频(0.1MHz-40MHz)时谐波失真严重,即使调整寄存器设置也无明显改善。建议检查输出电路设计,确保负载为50欧姆,并在电压合规范围内操作。
AI Generated Content
输出10MHZ,有20MHZ谐波输出,依次类推,输出11MHZ,有22MHZ。请帮助解答。
clock and timing
Clocks & Timers
Direct Digital Synthesis (DDS)
ad9910
Parents
beiszj
on Jul 25, 2025 2:21 AM
0
调试AD9957遇到同样问题,请问您是如何解决的?
Cancel
Up
0
Down
Reply
Verify Answer
Cancel
Reply
beiszj
on Jul 25, 2025 2:21 AM
0
调试AD9957遇到同样问题,请问您是如何解决的?
Cancel
Up
0
Down
Reply
Verify Answer
Cancel
Children
No Data