ADRF6755锁相环问题

1、最近在调试一款ADRF6755的芯片,在调试的过程中刚开始上电锁相环是好的 ,频率能够很稳定的输出,但是过了一会就突然间的就没有了,而且测试RESET脚是0.45V,锁相环的CP脚的输出是300-400mv,

2、请求解答一下如何能够降低6755的功耗电流,6755的有自身的电压输出3.3V,如果我用外部的电源3.3V是否对功耗能够减少?

3、对于I/Q两路的布线(阻抗50)如何做到两路的非常完美的匹配

4、6755对于输入的信号是否有幅度要求?差分的输入在不是很一致的情况下6755还会有很好的抑制么?

Parents
  • 您好!

    您测量到的是本振信号没有了吗?建议您先通过MUXOUT和锁定指示检查锁相环是否真正锁定。如果确定锁定后,还失锁,那么请检查在这段时间内,电源,地,参考输入信号是否有干扰信号。此外,还应检测MCU是否向ADRF6755写入了其他控制字。对于IQ的布线,应保证对称。对于IQ平衡和边带抑制可参考附件内文档。

    AN-1100.pdf
Reply
  • 您好!

    您测量到的是本振信号没有了吗?建议您先通过MUXOUT和锁定指示检查锁相环是否真正锁定。如果确定锁定后,还失锁,那么请检查在这段时间内,电源,地,参考输入信号是否有干扰信号。此外,还应检测MCU是否向ADRF6755写入了其他控制字。对于IQ的布线,应保证对称。对于IQ平衡和边带抑制可参考附件内文档。

    AN-1100.pdf
Children
No Data