ADRF6755锁相环问题

1、最近在调试一款ADRF6755的芯片,在调试的过程中刚开始上电锁相环是好的 ,频率能够很稳定的输出,但是过了一会就突然间的就没有了,而且测试RESET脚是0.45V,锁相环的CP脚的输出是300-400mv,

2、请求解答一下如何能够降低6755的功耗电流,6755的有自身的电压输出3.3V,如果我用外部的电源3.3V是否对功耗能够减少?

3、对于I/Q两路的布线(阻抗50)如何做到两路的非常完美的匹配

4、6755对于输入的信号是否有幅度要求?差分的输入在不是很一致的情况下6755还会有很好的抑制么?