Post Go back to editing

求助ADF4360-9与ADL5534的使用及设计方案问题?

现在想用ADF4360-9做个时钟源,输出功率20dbm以上,中心频率100Mhz,请问ADF4360的输出是否可以直接连接到ADL5534的两个输入端,让ADL5534作为一个放大器使用?这种方式能实现功率放大吗?

另外,ADL5534两个输入合并为一个放大器使用时,其Gain是一个的两倍还是仍为20dB?请专家给予指导,方案框图如下。

Parents
  • 你好,我们现在需要采用ADF4360-9进行锁相环设计,我们参考了评估板给出的原理图,也就是ug-106的第9页和第十页,但有些地方没有看懂,首 先是电源部分,原理图将USB正5V电压通过ADP3300-3产生VDD和VVCO电压,分别给DVDD、AVDD和VVCO供电,但很奇怪的是为何要 使用那么多的0欧电阻,如R1,R13,R24,R2和R27。另外,UG-106中第三页给出的PCB貌似和实物图不同,其中没有R39和D5,难道是 焊在背面?同时,在参考原理图和PCB中,三阶的环路滤波器部分的R10的位置应该如何选择,即放在背面什么位置,对环路滤波器有没有影响啊?谢谢

Reply
  • 你好,我们现在需要采用ADF4360-9进行锁相环设计,我们参考了评估板给出的原理图,也就是ug-106的第9页和第十页,但有些地方没有看懂,首 先是电源部分,原理图将USB正5V电压通过ADP3300-3产生VDD和VVCO电压,分别给DVDD、AVDD和VVCO供电,但很奇怪的是为何要 使用那么多的0欧电阻,如R1,R13,R24,R2和R27。另外,UG-106中第三页给出的PCB貌似和实物图不同,其中没有R39和D5,难道是 焊在背面?同时,在参考原理图和PCB中,三阶的环路滤波器部分的R10的位置应该如何选择,即放在背面什么位置,对环路滤波器有没有影响啊?谢谢

Children
No Data